Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to save the communication and operation report of an explicit communication like Read_Var EF using an ST section

In the Control Expert documentation, you can see the below :
doc CE
See below an example of an ST section that will record the communication and operation report value of an explicit communication EF (So the Management_Table[1] of this EF) and will check and reset accordingly the function management parameters  :

st

This ST section is also available in attachment

Schneider Electric Saudi Arabia

Attachment(s)
( Read_Var ETH ).txt [888 Bytes]
St section.zip [974 Bytes]