Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does EcoStruxure Control Expert support bit extraction of a DINT, DWORD and UDINT data type?

Issue:

Bit extraction of DINT, DWORD and UDINT data type in Ecostruxure Control Expert

Product Line:

EcoStruxure Control Expert

Resolution:

As of Control Expert V15.3, bit extraction of a DINT, DWORD and UDINT data type is allowed. Prier to this version it was not allowed.

image1