Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there library/function block or template to add ATS480 soft starters to be controlled in Ecostruxure Machine Expert?

Issue:

How to program ATS480 using FB with EcoStruxure Machine Expert?

Product Line:

EcoStruxure Machine Expert

ATS480

Environment:

Ecostruxure Machine Expert

Cause:

There is a DFB and some information for Ecostruxure Control Expert.

Resolution:

There is no specific FB for the ATS480. Also the ATS480 DTM is not integrated yet on Machine Expert.

It is possible to use Generic Modbus TCP Slave for controlling ATS480 (so, no FBs as for ATV).

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre