Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATS480 PTC / PT100 Connections and monitoring status via communication options.

Customer is connecting PTC sensors to the ATS480 soft start and wants to know how to read the thermal value from that circuit to monitor the actual motor temperature.

The ATS480 allows the connection of PTC or PT100 sensors using the PTC1/AI1, PTC2, PTC3 and COM terminals.

ptc

There are several parameters that can be monitored over a network....depending on the type of sensor being used.

  • TH1F and TH1A are used only when AI2T=PT100, or 3 PT100

d

The temperature correspondence used in drive when AI1T=PT100 or 3PT100 are a standardized value. See Spec below :

a

The Standardized value is available from parameter AI1C: Logic Address 5232.

  • When AI1T=PTC, it is not possible to know the temperature. they fixed by the sensors manufacturer, so not configurable by the customer:

d

PTC must follow our recommendation:

s

The Physical value of AI1 can be read from parameter AI1C: Logic address 5242.

So, you must to read the value in Ohm then make your conversion in PLC using the curve provided by PTC manufacturer.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)