Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Troubleshooting Geo SCADA Dongle Issue: Understanding Error Code 9 and Resolving It

Sometimes, when a Geo SCADA dongle is plugged in, the light turns green briefly and then shuts off. When trying to obtain a locking code in the Field Exchange utility, the following error message appears 'Could not find key! Error Code is 9.'

Error code 9

This error indicates that either the dongle is not connected to the machine, or it is not being detected. If the dongle is plugged in and worked on another machine, it’s possible that IT has disabled the USB ports as a security measure.

To resolve this issue, please check the connection and ensure the dongle is properly recognized by the machine.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre