Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EcoStruxure Power Operation/Power SCADA Operation: ION protocol wrong credentials entry on EPO/PSO side can cause meter front panel lockout

Issue

This is related to EPO/PSO ION driver communicating with ION7650 and PM8000 meters over ION protocol. This is applicable to the meters' firmware which supports standard and advanced both security options. If the user selects the standard security on meter side, and enters wrong password on EPO side the meter will start logging front panel auth fail errors and locks out eventually. In standard security mode we have only one user in meter, so this stops the user from accessing the meter front panel but we can connect to the meter using telnet/SSH.

Meter logs showing front panel auth fail events

Meter status still shows good quality on EPO side even though the password entered is wrong.

EPO status while meter password entered is wrong in citect ini parameters

Environment

EcoStruxure Power Operation/Power SCADA Operation with ION driver and PowerLogic or ION meters with firmware supporting standard security version

Below is an example architecture where multiple devices are communicating to EPO/PSO over ethernet via ION protocol and upon this scenario, the operator may not be able to access front panel once its locked out.

Architecture

Cause

The meter expects correct username and password for the corresponding UserID. For example, below is wrong password set (correct one was 0) on citect.ini parameters for UserID 0 which is used in ION7650 meter

EPO citect ini settings with wrong password example

There is setting in the meters which governs lockout and can be seen below for ION default is 8 attempts after which it locks out. Settings can be accessed from setup assistant and edit security settings.

Meter settings in ION setup for standard security

Meter security lockout settings

Resolution

While setting ION protocol in EPO/PSO, set the below citect.ini parameters correctly as per meter userID and credentials. Note that ION7650 uses UserID 0 as default and PM8000 uses UserID 1. Meters have default passwords 0 but it should be confirmed on meter side for the current credentials.

Also, it is possible to set ION protocol INI parameters for the entire Power Operation system or for a specific cluster or IO server or device if different credentials are used for different devices.

Example:

PROTOCOL.MYCLUSTERNAME.IOSERVER.DEVICE_Name

[ION.MYCLUSTER.IOServer.DEVICE_A]

UserID=0

Password=0

And for entire PO,

[ION]

UserID=0

Password=0

Upon using the correct credentials, meter logs show no more auth fail errors and prevents lock out.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre