Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Batch Trigger Unavailable Error in Realflo.

How can I resolve a "Batch trigger unavailable" message in Realflo similar to the image below?

Batch trigger unavailable

Answer:

A coil, status register, or database object triggers batch operations. The batch starts when the batch trigger transitions from OFF to ON, and stops when the batch trigger transitions from ON to OFF.

The common issue was that the Batch Trigger Object Name wasn't defined or assigned in the RemoteConnect object database. The Batch Trigger Object Name can be found in the Realflo RUN configuration under the Batch/Well Test tab. This Batch Trigger Object Name must be assigned in the RemoteConnect object database.

batch trigger 2

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre