Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is APC Portable Power Station (Schneider OffGrid)?

Issue:
What is APC Portable Power Station (Schneider OffGrid)?

Product Line:

  • Schneider OffGrid Portable Power Station models: PPS330, PPS500, and PPS730

Resolution:
APC Schneider Electric's OffGrid Portable Power Station is designed for outdoor enthusiasts and home users to provide consistent, reliable power whenever you need it - anytime, anywhere.
It is a versatile battery-powered device designed to provide reliable power for various applications, especially in off-grid situations or during power outages. Here are some key features:

  • Portability: Lightweight and compact design, making it easy to transport.
  • Multiple Outputs: Usually includes AC outlets, USB ports, wireless charging, and DC outputs to power different devices simultaneously.
  • Rechargeable: Can be recharged using optional solar panel (add-on), wall outlets, or car chargers, providing flexibility.
  • Capacity: Varies by model, allowing for usage of small electronics like smartphones, laptops, lights, and even some appliances.
  • Safety Features: Often includes built-in protections against overcharging, overheating, and short circuits.
  • Sustainable: Sustainable packaging, casing made with 60% recycled plastic, and optional solar panels for eco-friendly recharging.

These power stations are ideal for camping, outdoor events, emergencies, or any situation where reliable power is needed away from traditional sources.



Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: