Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Battery Module Does Not Turn On in Smart-UPS Ultra 5-10kVA or Smart-UPS Modular Ultra

Problem: The SRYLBM battery module does not turn on in Smart-UPS Ultra 5-10kVA or Smart-UPS Modular Ultra, even after tightening the thumbscrew.

Product Line: SRYLBM

Environment: SRYLBM installed in the following UPS models: SRTL5KRM2UI, SRTL5KRM2UT, SRTL8KRM4UI, SRTL8KRM4UT, SRTL10KRM2UI, SRTL10KRM2UT, SRYLxxKxxRMXLT

Cause: The switch on the battery module does not fully engage after tightening the thumbscrew.

Resolution: Use a flat head screwdriver to tighten the thumbscrew further until the battery module turns on.

IMPORTANT: Tighten with caution as over tightening may damage the thumbscrew.

img

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre