Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Link a VIM (Voltage Interface Module) to one of our Avatars Loads in TeSys Island

Product Line:
Industrial Automation Control

Environment:
Motor Management Systems  TeSys Island

Cause:
What´s the correct path to add a Voltage Interface Module on of my avatar Loads

Resolution:

Voltage Interface Modules will require to be added to a specific Load Avatar in order to be mapped on the TeSys Island topology, to add this module, the correct path will be to first add our Load , it can be a standard starter or a SIL starter:

We will need to add a LOAD to My Avatar

Add Avatar TeSys Island

To load our VIM we will need to add the Load Energy Monitoring in our Avatar Parameters window

Load Energy Monitoring TeSys Island

This will automatically add the Voltage Interface Module to our LOAD and will be added to the Avatar Topology:

Physical View TeSys Island

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: