Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Logic Editor does not appear Available in RemoteConnect

Problem:

When opening up a project, a user might notice that there is no way to access the SCADAPack x70 Logic Editor, despite being sure that the project contains a logic component. There is no "Open Logic Editor" button.

"Open Logic Editor" button does not appear

Solution:

Starting with RemoteConnect version 3.2.2, the software comes with a Maintenance Tool version. It is a smaller download and simpler install to allow a technician in the field to upload and download a project to an x70 controller but does not allow the user to make changes to the logic or changes to objects that might affect the logic

From both the Start Menu, and when opening RemoteConnect, there is no immediate indication that it is running as a Maintenance Tool. Please go to the question mark icon and select About... to confirm if it is the Maintenance Tool

About window shows it as Maintenance Tool

The user may have downloaded and installed "TBUM250348 RemoteConnect Maintenance Tool Rx.y.z.zip" where x.y.z indicates the revision number. If a user has downloaded the Maintenance Tool, they will need to download the full version if they wish to use the Logic Editor and make changes that might affect the logic.

Alternatively, the full download "TBUM250347 RemoteConnect and SCADAPack X70 Utilities Rx.y.z.zip"  contains both the full version and the Maintenance Tool version of RemoteConnect. During installation, the user may have inadvertently selected the Maintenance Tool installation.

Options available during setup

The user will need to install the full version along with Control Expert in order to use the Logic Editor and make changes that might affect the logic.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre