Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VSD in PrismaSeT I

VSD- Variable Speed Drive can be installed in PrismaSeT I Floor Standing switchboards.

Ratings starting from 0.37kW upto 110kW can be installed in IP42/54 configuration with forced cooling for an ambient ≤ 35°C.

For ambient >35°C, Type- 2 co-ordination chart can be referred.

Fan and Filter CR# with module size as per kW rating is available in EasyPrisma Software.

Note- Global door should be mandatorily plain for VSD feeders. Do Not use Glass door as you will not be able to make cut out for the fan and grills.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre