Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to avoid interference of device handles with door in PrismaSeT I Switchboard

!!!Confidential Content

The available space behind doors in PrismaSeT I is as shown below in image for a typical combination of W600+400 cubicle.

available space behind door

Fig. 1

In the W600 compartment, the space available between door and front plate is 63mm. In W200/300/400 compartment, space available behind the door depends on the orientation of Form 2 partition and hence it can be 64.5mm or 40mm.

available space behind door

Fig. 2

The length of any device handle or LOTO arrangement projecting outside the front plates shall be less than this gap available behind the doors and it should not hit the door. Example: As in below image the distance between the front plate and edge of rotary handle is 42.3 mm which is lesser than the space available behind the door. So, its possible to use this handle safely without impacting the door.

device dimension

Fig. 3

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre