Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What generation of processor is needed to install Control Expert 16.1?

For installing Control Expert 16.1, the generation of the Intel Core processor does not matter, as long as the frequency is greater than 3 GHz.

Image