Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to export I/O variables from one Control Expert project to another?

Issue:

What are the alternatives available and the correct procedure to export/import IO variables coming from different I/O modules?

Product:

M340,M580 controllers

Environment:

EcoStruxure Control Expert software (previously Unity Pro)

Resolution:

When addressing the inputs and outputs of an I/O module, the following options can be selected:

I/O data type: Topological

I/O data type: Device DDT

  • If using I/O data type: DDT

For Control Expert, when inserting the module and selecting DDT addressing the variables are generated automatically:

ExportTopological_1

ExportTopological_2

Here it is necessary to add the modules in the new project and select the data type I/O: DDT to generate the variables.

  • I/O data type: Topological

If Topological Address is used, an export of the variables and import of them in a new project is possible, but it is necessary to have the same type of module in the same rack slot of the new project.

Example:

There is an Analog Output module BMXAMO0802 with assigned variables manually in the I/O Objects tab (double click module -> select BMXAMO0802 -> I/O object tab is available)  , to export these variables and import them in a new project, the new project needs to have the same type of module in the same slot. See the next images:

ExportTopological_3

ExportTopological_4

Note: XSY file was exported

ExportTopological_5

ExportTopological_6

ExportTopological_7

ExportTopological_8

If the module is in a different rack or slot, it is necessary to modify the address of the variables. An example of the different syntaxes is shown below:

I/O Topological Notation for Direct Addresses.

  • %I0.4.5 = Rack 0 slot 4 input 5 (Premium, M340, M580)
  • %Q1.4.5 = Rack 1 slot 4 output 5 (Premium, M340, M580)
  • %IW\2.3\1.4.5 = bus 2 RIO drop 3 rack 1 slot 4 Analog Input 5, of (Quantum)
  • %IW\3.50\0.0.1.5 = bus 3 device 50 of mod 0 of rack 0 channel 1 Data 5.

  • Unity Variables Management tool

There is an excel tool for Control Expert, in which it is possible to export variables and insert them in the Excel file, and here it is possible to make a modification of the variables, create or delete variables in a simpler way, then it is only necessary to export the file made in excel and import it again to Control Expert:

The Excel file with a macro generates an .XSY file that then can be used to import into the Control Expert:

ExportTopological_9

ExportTopological_10

ExportTopological_11

FAQ: Is there any tool could define/modify the .xsy file?

Link: https://www.se.com/ww/en/faqs/FA267997/

FAQ: How to manage Unity Pro variables in Excel

Link: https://www.se.com/us/en/faqs/FA283809/

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre