This can occur if the regional setting for the windows clock is incorrectly set or set to use cyrillic letters
It is recommended to ensure that the regional settings for the Windows clock on the PC' is correctly set.
Released for: Schneider Electric Saudi Arabia