Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
NLP status on an ATS480

NLP indicates that the unit has no run command, and no main power supplied on L1/L2/L3.

On this softstart, CL1 and CL2 will be needed as hot and neutral 120V control power. With only this power supply provided, the unit will state NLP.