Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I connect to Twido PLC using EcoStruxure Machine Expert Basic?

Issue:

I know that Machine Expert Basic can open and convert a TwidoSuite project file, but can Basic actually connect to and upload from a Twido?

Product Line:

Twido PLC

Environment:

EcoStruxure Machine Expert Basic

Cause:

N/A

Resolution:

Ecostruxure Machine Expert Basic can open and convert a Twidosuite program, but is used only to connect to M221, M200, M100, TM3 and TM2 modules.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre