Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change power up alarm behavior for ION9000, PM8000 and ION7400 meters

Issue
Meter's Power up alarm changed behavior in V3.1.0 and is now active for 1 day. Would like to change the behavior of the alarm either disable this alarm or change the duration of the alarm.
Note that this alarm is required for meter to meet WELMEC compliance. If the meter needs to meet WELMEC compliance, do not change the alarm behavior.

Products
ION9000, PM8000, ION7400 V3.1.0 template and later

Environment
ION Setup or Power monitoring Expert PME Designer

Resolution
The alarm is from setpoint module #1 "Pwr up". This setpoint module is linked to One Shot Timer module #12 "PwrUpToBool"
To de-activate the alarm, change the setup register of the Setpoint module. The Enable register could be set to "Disabled".
To change the duration of the alarm, change the duration setup register of the One Shot Timer module. The default of 86,400 is 1 day (3600*24), change the duration to meet need.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre