Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the communication between a BMENOP0300 module and an C264 device ?

To configure a C264 device, we use the PACIS SCE tool to generate a ZIP configuration file, which is then transferred to the C264 device using another software called PACIS CAT.

It is mandatory to use this same ZIP file to configure the BMENOP0300 module, by extracting the .SCD configuration file from it and using the Modicon IEC61850 Configuration tool to transfer it to the module.

schema

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: