Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the alternative or replacement of A9A26929 (Obsolete)?

A9A26929 was already obsoleted and replaced by either:

A9A26909 (Standard Application) - Auxiliary contact, Acti9 A9A, iOF/SD+OF, 2 C/O, 100mA to 6A, 24VAC to 415VAC, 24VDC to 130VDC, top and bottom connection

Datasheet | Instruction Sheet | CAD Files

or

A9A26919 (PLC Application) - Auxiliary contact, Acti9 A9A, iSD+OF, 2 C/O, 2mA to 100mA, 24VAC to 250VAC, 24VDC to 220VDC, top and bottom connection

Datasheet | Instruction Sheet | CAD Files

For more product substitution, you may refer to the FAQ below:

Singapore: https://www.se.com/sg/en/faqs/FAQ000264549/

Malaysia: https://www.se.com/my/en/faqs/FAQ000264549/

Philippines: https://www.se.com/ph/en/faqs/FAQ000264549/

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: