Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Smart UPS Modular Ultra SRYLBM does not turn on in the External Battery Pack

Issue:

The XRCC (External Battery Pack Communications Card) is solid green, but a known good SRYLBM does not power up (UPS does not recognize BM) in the XBP (External Battery Pack).


Product Line:

Smart UPS Modular Ultra


Environment:

All models, all serial numbers


Resolution:

There is possibly a problem with the signal going from the UPS to the XBP.  When you plug the XBP connector into the UPS frame and engage the thumbscrew, it should close the switch to complete the circuit and allow the BMs in the XBP to turn on.  Check to see if the thumbscrew is fully engaged.  You may need to use a screwdriver to fully engage the switch.

XBP connector

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre