Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Error 1720 gets returned when trying to install a new version of Control Expert on top of an older version.

The following error gets returned when trying to install a newer version of Control Expert on top of an older version.

Error 1720. There is a problem with this Windows Installer package. A script required for this install to complete could not be run. Contact your support personnel or package vendor. Custom action UP_TopologyManager_Service_Check script error -2146828275, Microsoft VBScript runtime error: Type mismatch: 'Session.Property' Line 25, Column 2,

To resolve the issue,

  • Open the folder named 'C:\Program Files (x86)\Schneider Electric'
  • Delete the folder for the old version of Control Expert.
  • If the folder cannot be deleted, resolve the trusted access rights issue and retry.
  • If the folder still cannot be deleted, open the Control Expert folder and delete the contents.
  • Reboot the PC.
  • Mount the installation  iso file for the older Control Expert version.
  • Run setup as an administrator.
  • Select Repair.
  • Reboot the PC.
  • Mount the installation iso file for the older Control Expert version.
  • Run setup as an administrator.
  • Select Remove.
  • Reboot.
  • Install the newer version of Control Expert.