Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VarPlus Logic VL 6 - can the firmware be upgraded?

Issue

Can the firmware for the VarPlus Logic VL 6 be upgraded?

Product Line
VarPlus Logic

Environment

Firmware


Resolution

The VarPlus Logic VL6 firmware is not field-upgradable. The current firmware version is 001.000.002.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre