Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When configured with multiple vSAN clusters, PowerChute Network Shutdown fails to disable HA and vCLS all the clusters.

Issue:

PowerChute Network Shutdown has been configured to shutdown multiple vSAN clusters and HA/vCLS is only disabled on one cluster.

Product Line:

PowerChute Network Shutdown versions 5.0, 5.1.

Environment:

VMware vCenter 7 or 8 configured with multiple vSAN clusters.

Cause:

PowerChute can only disable HA and power off vCLS for a single cluster.

Solution:

Install multiple instances of PowerChute. One for each cluster.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre