Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Smart UPS Modular Ultra shows RS232 Communication Entry

Issue:

The UPS shows RS232 comm alarm detected 140B-0000 entry every few seconds on the display and power event log.

Example of the event log:

10/01/2024    13:34:26    Device    RS232 comm alarm cleared [140A-00A0].    0x02B8
10/01/2024    13:34:25    Device    RS232 comm alarm detected [140B-00A0].    0x02B9
10/01/2024    13:31:25    Device    RS232 comm alarm cleared [140A-00A0].    0x02B8
10/01/2024    13:31:25    Device    RS232 comm alarm detected [140B-00A0].    0x02B9
10/01/2024    13:28:25    Device    RS232 comm alarm cleared [140A-00A0].    0x02B8
10/01/2024    13:28:25    Device    RS232 comm alarm detected [140B-00A0].    0x02B9
10/01/2024    13:25:25    Device    RS232 comm alarm cleared [140A-00A0].    0x02B8
10/01/2024    13:25:24    Device    RS232 comm alarm detected [140B-00A0].    0x02B9
10/01/2024    13:22:24    Device    RS232 comm alarm cleared [140A-00A0].    0x02B8
10/01/2024    13:22:24    Device    RS232 comm alarm detected [140B-00A0].    0x02B9


Product Line:

Smart UPS Modular Ultra


Environment:

All models, all serial numbers


Resolution:

The firmware has been improved to correctly handle the situation that causes the entry to appear repeatedly in the log.

Please upgrade the UPS to at least firmware 17.0, then clear all alarms if needed.

In order to upgrade the UPS properly, please use the following FAQ - https://www.apc.com/us/en/faqs/FAQ000261838/

If the alarm returns after upgrading the firmware, please contact support.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre