Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Troubleshooting Python Driver for Geo SCADA 2025.

This article will cover the various errors that may be encountered while running the Python driver on Geo SCADA 2025 and later versions:

One common issue is a pop-up error message stating: "Operation was unsuccessful." This may appear during the execution of the Python program

error 1

This usually indicates that either the Python executable is not installed or it is not correctly referenced in the server configuration tool: (The Python executable is located in C:\Program Files\Python313)

server config

When installing Python, it is recommended to check the 'Use Admin Privileges when installing py.exe' box to grant admin privileges to Python executable files. Additionally, selecting 'Add Python.exe to PATH' is advisable to add the Python path to your environment variables, allowing you to execute Python commands from the Windows command line.

Note that Geo SCADA supports python versions 3.12 and 3.13

python

If you encounter the error ModuleNotFoundError: No module named 'geoscada' while running your Python program, it means that Python cannot find the Geo SCADA API.

error 2

In order to resolve this, install the Geo SCADA Expert API Python package files by executing the following commands in the Windows command line:

cd C:\Program Files\Python313 (depends on the python file location)

and

python -m pip install --force-reinstall --find-links="C:\Program Files\Schneider Electric\ClearSCADA\PythonPackages" geoscada-client

If the issue persists and you see the message "defaulting to user installation because normal site-packages is not writeable" after running the command, please verify that the command was ran as an administrator and that the site-packages directory is writable.

error 3

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre