Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What should I check when the XVR3 series does not work ?

The possibilities are as follows:
-The wiring may not be correct.
Please check the wiring is correct based on the instruction sheet.
If the wires have been terminalized, please check that there are no problems with the processing.
-The product may not be receiving the correct power voltage.
Please check that the power supply is set to the correct voltage and has sufficient power capacity.
(We recommend that you measure the voltage at the product's wiring using a digital multimeter.)

If the above does not resolve the issue, remove the product from the control device and check the product alone.
If it still does not work, the product may be broken.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre