Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Shipping Display Cover Removal for Newly Installed 5K and 6K SRT UPS Units

Procedure:
Shipping Display Cover Removal for Newly Installed 5K and 6K SRT UPS Units

Product:
APC by Schneider Electric SRT 5KVA and 6KVA units or UPS SKU numbers beginning with SRT5K or SRT6K - All regions

Solution:
An SRT 5K and 6K UPS will come with a metal cover for its screen upon unboxing.

The following shows a set of images of the display cover and how it is found on a newly unpacked UPS

The reason behind this is that the screen is attached directly to the battery door of the UPS and accidents can occur at first time installing the batteries if the UPS as the door can swing and make the screen bump and possibly cause permanent / physical damage. This is most common on SRT 5K and 6K UPS chassis.

In order to remove this cover, one must first locate 4 screws from the battery door and 1 from the metallic cover itself (to prevent it from swinging open). These screws will need to be removed.

The following shows a set of images of the screws that needs to be removed during the process

Once the screws have been removed, the battery door can be slid to the left to be unlocked. After unlocking it, the battery door will be able to swing open which in turn can allow you to remove the screen metallic cover from being latched onto it.

The following shows a set of images that shows how the display cover can be removed after opening the battery door

If you have any clarifications and/or requests for the above-mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.