Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
FAQ: What are the meanings of Accuracy and Repeatability as found on the ETE datasheet?

Accuracy: The measure of how close a measurement gets to the actual (true) value.

Repeatability: The consistency of the sensor's readings when the same measurement conditions are repeated multiple times. This is an aspect of precision.

Accuracy and Precision

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre