Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unable to Connect PAS with Certain Mobile Devices (Motorola & Vivo)

If you're having trouble connecting to PAS using Motorola or Vivo smartphones, try the following:

  1. Disable Mobile Data:
    Turn off mobile data or temporarily disable the SIM card’s data connection
  2. Reconnect to PAS:
    After disabling mobile data, attempt to connect to PAS again—either by scanning the QR code or using the manual connection method.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: