Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is Multilanguages Online Help Available in Control Expert v16.2 ?

Issue: The Control Expert v16.2 online help is delivered in English for all GUI languages. Some customers want a translation of the Control Expert Online Help into other languages.

Product Line: EcoStruxure Control Expert

Environment: EcoStruxure Control Expert v16.2

Resolution: To support better usage in other countries, translated versions of the online help are provided in French, Italian, German, Spanish, and Chinese in Control Expert v16.2. The customer does not need to install a Hotfix. The multilingual feature is integrated into the v16.2 setup.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre