Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SCADAPack x70 Modbus Scanner Status Objects
When using the Modbus Scanner, the communication status is represented by a read-only object that reflects the current state of communication with a Modbus RTU Server or Modbus/TCP Server1. This status object is named in the format MBUS_DeviceName_CommStatus.
Modbus Scanner Communication Status Object
Here's what the different status codes for communication status mean:
0 - Device not found: The Modbus device could not be located.
1 - Trying to contact device: The system is attempting to establish contact with the Modbus device.
2 - Initializing device: The Modbus device is currently being initialized.
3 - Communications with device were unsuccessful: Communication attempts with the device have failed.
4 - Device is online: The Modbus device is successfully communicating and online.
5 - Device is disabled: The Modbus device has been disabled.
These status objects are part of the information provided by the Modbus RTU Client or Modbus/TCP Client operations when the Modbus Client options are enabled in the RemoteConnect project settings.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre