Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
"Unable to build the logic application" error in RemoteConnect

Problem:

Unable to write RemoteConnect application to SCADAPack x70 RTU due to "Unable to build the logic application" error.

Unable

Solution:

Check the logic application in the Logic Editor to ensure it is properly built by updating and building the logic. If the logic application is not built and there is an error during the update and build process, then correct the problem indicated in the program.