Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you save the ATV320 Drives program with function blocks using the Multiloader device?

Issue:

Saving the ATV320 Drives program with function blocks on the Multiloader programmer.

Product Line:

ATV320 with Multiloader device.

Environment:

All

Cause:

Getting an error message when trying to download the ATV320 program with function block using the multiloader.

Resolution:

When the ATV320 has ATVLogic running, you must stop the ATVLogic running before any multiloader transfer (you must set fbCd=STOP via keypad using ATV320 integrated Jog dial). Otherwise, the transfer will not be done.

Menus

-Config

-Full

-Function blocks

-FB command (fbCd)

set to Stop.

Now you can download the ATV320 program into the Multiloader.