Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the recommended minimum bending radius for the BMXFCW303?
  1. What does “minimum bending radius” mean?
    The minimum bending radius is the smallest radius you can safely bend a cable without damaging it or affecting its performance.

  2. What is the recommended minimum bending radius for the BMXFCW303?
    The minimum bending radius for BMXFCW303:

    • Static application: 15 × D
    • Occasionally moving: 20 × D

Note: "15 × D" means 15 times the cable diameter.

Improve
CtrlD

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: