Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Offer: What is the warranty of the EcoStruxure Transformer Sensor?

A lifetime warranty is provided on the Sensor with replacement hardware provided free of charge while a subscription to EcoStruxure Transformer Expert is active.  Returns must be authorised by contacting support.dts@se.com. See the EcoStruxure Transformer Expert Datasheet for more information.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre