Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Transformer: What is temperature rise in a transformer?

Transformers do not perfectly convert power. Some energy is lost in the process. This energy heats the transformer. As the temperature rises it causes changes within the transformer which degrade performance.   All transformers have a maximum safe operating temperature. They also have a maximum safe rate of temperature change under high instantaneous load conditions.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre