Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Transformer: What test results indicate normal operation and what can indicate a fault?

If the water content in the transformer oil is within the IEEE standard specified limits, then, we can be comfortable with its operating condition. Violating the standard limits may result in fault conditions. The same applies for temperature measurements.

The EcoStruxure Transformer Expert solution provides the exact data for temperature as well as the water content in oil and hence indicates normal or risky operating conditions.