Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Offer: What is the price of the solution?

The EcoStruxure Transformer Expert sensor is included with the subscription to the EcoStruxure Transformer Expert Dashboard.  Pricing is based on a 3 or 5 year subscription.  Discounted up-front payments are available if users prefer to capitalise the cost of a subscription over a number of years.  Contact Schneider Electric or your local Schneider Electric partner for detailed information.