Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there protection recommendation with fuse for the input channels on TM3AI4?

Issue:

What protection is needed for the input channels on TM3AI4 from overcurrent or overvoltage?

Product Lines:

TM3

Environment:

PLC software configuration in EcoStruxure Machine Expert

Resolution:

There is no protection recommendation with fuse for the Input channels except the use of shielded cables and the connection of the shield to the FE:

Shield cable