Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does EPC-M crash when "Skip Password" is selected with PAS?

The crash occurs when EPC-M version 2.2.0 is used with PAS firmware version 2.3.0 and the user selects the "Skip Password" option. This behavior is due to incompatibility between these versions and a failure to meet the RED DR cybersecurity compliance requirements.

To avoid this issue:

  • Upgrade EPC-M to version 2.3.0 when using PAS 2.3.0.
  • If using EPC-M 2.3.0 with PAS 2.2.0, it is recommended to upgrade PAS to version 2.3.0 for full compatibility and RED DR compliance.

Firmware Compatibility Table

SL NoEPC-M VersionPAS FW VersionRED DR ComplianceCommentsRecommendation
12.2.02.2.0NASKIP Password option availableNA
22.3.02.3.0Fully CompliantIt is mandatory to set a password.NA
32.2.02.3.0Non-CompliantThe app may crash when "Skip Password" is selectedUpgrade EPC-M to version 2.3.0
42.3.02.2.0PartialRecommended upgrade for stable supportUpgrade PAS firmware to version 2.3.0