Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many wireless batteryless push buttons(ZBRT1/ZBRT2) can be connected to the EcoStruxure Panel server?

The maximum number of devices that are compatible with the EcoStruxure Panel server depends on the panel server version. PAS400 is compatible with max of 20 pushbuttons. The PAS600* and PAS800* versions are compatible upto100 wireless batteryless pushbuttons.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre