Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I install Control Expert 16.2 and EAE 24.1 in a same OS ?

Issue

Can I install Control Expert 16.2 and EAE 24.1 ( EcoStruxure Automation Expert  ) in a same OS ?

Product Line

Control Expert, EAE

Environment

Control Expert 16.2 , EAE 24.1

Resolution

It is not suggested to install EAE 24.1 and Control Expert 16.2 in the same OS at the moment , compatibility testing will only be confirmed with Control Expert 16.4 or higher version, scheduled to be released around Q2 2026. Once Control Expert 16.4 or higher is released, both EAE and Control Expert can be installed in the same OS.