Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to retrieve log files from a controller in EAE BT

1.Open EAE Buildtime and load the EAE Solution currently running on your controller.

2. Navigate to the Deploy & Diagnostics tab.

3. Log in to the device.

4. Expand the Action tab for your controller, then go to Log File > Fetch log files to retrieve the files.

M580d fetch log

5. Wait for the message: "Fetching of log file successfully finished."

action progress

6. Close the Device Log Viewer pop-up window.

7. Locate the cyclic.log and device.log files in the following path (also see note c. below)
Documents\Schneider Electric\EcoStruxureAutomationExpertProjects\<project_folder(s)>\IEC61499\Log

8. Send both files to Technical Support.

NOTES:

a. This Knowledge Article was made based on EAE version 24.1.

b. For SoftdPAC HA configurations, log files should be fetched from the parent controller menu to ensure that the cyclic and device logs for both the left and right iPCs are retrieved. Make sure to send all four files to Technical Support.

HA fetch log

c.  The path to retrieve the log files from your controller can also be retrieved from the Device Log Viewer pop-up window, by:

  • Clicking on File > Load Log
  • In the Open Log file window, right click on the folder address and click on Copy address as text

retrieve path

  • Open a File Explorer window, edit address and paste the one retrieved from the Log window. Press ENTER.

file explorer

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: