Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to retrieve Log Files from the CRD Head Module

1. Open EAE Buildtime and load the EAE Solution currently running on your controller.

2. Navigate to the Deploy & Diagnostics tab.

3. Log in to the device controlling the CRD head module.

4. Stop the controller by going to Action > Device actions > Stop from the Deploy & Diagnostics tab.

5. Go to the System tab, then Physical Devices, and click Start Monitoring.

1

6. Right-click on the CRD and select Fetch logs.

2

A pop-up message will confirm that the fetch was successful and display the file name and location.

3

7. Open File Explorer and navigate to the directory specified in the message. For EAE 24.1, the default location is:
C:\ProgramData\Schneider Electric\EcoStruxure Automation Expert 24.1\StudioLog

8. Send the file to Technical Support for analysis.

NOTE:

  • This Knowledge Article was made based on EAE version 24.1.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre