Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Residual Current Measurement "I calc res" Not Available on ION7400 and PM8000

Issue
The "I calc res" residual current value is not available in the Power Meter module outputs of the ION7400 and PM8000 meters, despite being mentioned "Residual current measurement" in documentation. This measurement is available on ION9000 meters, leading to confusion about its availability across platforms.

_____________________________________________________________
Product Line
Product Models: PM8000, ION7400
_____________________________________________________________
Solution

The ION7400 and PM8000 meters can only calculate residual current in a 4-wire configuration, using vector summation of inputs I1 to I4, with the result represented as I5 (i.e., I1 + I2 + I3 + I4) which is provided by the Power Meter Module’s output register called I5.

This register is also linked to the Data Mapping Meas 1 module, which defines the Modbus data labeled Current G with register number 3008 as described in the device’s Modbus register map, and is reflected on the meter’s display and web interface tagged as I5.

ION9000 includes a physical I5 input for direct residual current measurement where the ION7400 and PM8000 lack this hardware capability.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: