Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is SQL Server Browser Service Required for PME?

Issue

Is SQL Server Browser Service Required for PME?

Product Line

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Windows Services

SQL Server

Resolution

SQL Browser Service is a Microsoft SQL component used to assist clients in connecting to SQL server instances. It is most useful when there are multiple instances on a single machine or database server.

In cases where the PME system is standalone (application server and database server on one server) and there are not multiple SQL instances, SQL Server Browser Service can be disabled.