Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does my Small Epoxy Resin Transformer has a higher voltage secondary output ?

The small Epoxy Resin Transformers are designed with compensation in the Primary winding that guarantees that the output voltage will be fully 120V or fully 240V or whatever at rated Full Load Secondary Amperage.  This means that the Transformers will output slightly higher voltage on the Secondary when that winding is not loaded or connected to anything. The percentage varies with design and VA size, but on this Transformer it should be about 4% to 5%. The incoming voltage, if a bit high will also increase the output on a small Transformer.

If the voltage is slightly higher than mentioned, please contact Tech Support for further advice.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre