Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SAGE RTU Latest Firmware Available

Issue:

Users need access to the latest secure firmware for SAGE RTU devices.

Product:

SAGE RTU

CPU C3414

Environment:

SAGE RTU units using C3414 CPU (Red board)

Secure environments requiring updated firmware for compliance and functionality

Cause:

Users require the latest firmware to ensure security, compatibility, and optimal performance of SAGE RTU devices.

Resolution:

The latest firmware for the SAGE RTU is available at the following link:

https://www.se.com/us/en/download/document/C3414-500-S02K5_P9_Firmware/

It only applies to CPU C3414 (secure) versions.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre